What are RoHS and RoHS2.0?

Modified on Fri, Jun 19 at 12:50 PM

It is a law that restricts (prohibits) the content of the target substance (group) above the regulation value.
・If there is no alternative method other than using the target substance (group), exemption use is permitted.
1, RoHS (2011/65 / EU) (RoHS6 substance in HRS)
Substances: (1) Cadmium (Cd), (2) Lead (Pb), (3) Mercury (Hg), (4) Hexavalent chromium (Cr6 +), (5) Polybrominated biphenyls (PBBs), (6) Polybrominated diphenyl ethers (PBDE) Kind)
Regulation value: Cadmium (Cd) 100ppm (0.01%) and 5 other substances 1000ppm (0.1%)
2, RoHS2 (EU) 2015/863 (RoHS10 substance in HRS)
Substance group: (1) cadmium (Cd), (2) lead (Pb), (3) mercury (Hg), (4) hexavalent chromium (Cr6 +), (5) polybrominated biphenyls (PBBs), (6) polybrominated diphenyl ethers ( PBDEs),
(7) Bis phthalate (2-ethylhexyl) (DEHP), (8) Butyl phthalate (BBP), (9) Dibutyl phthalate (DBP), (10) Diisobutyl phthalate (DIBP)
Regulation value: Cadmium (Cd) 100ppm (0.01%) and 9 other substances 1000ppm (0.1%)