There is an error with Chem SHERPA.

Modified on Fri, Jun 19 at 12:50 PM

Please check the type of error.

In case of "Warning"

Warning: Primary Article Identifier is entered but Material Category is not selected. If it is SCIP eligible, select it.

--> Material Category is the substance content concentration condition of SCIP registration
(more than 0.1% of articles as such) is not met.
No input is required.

* It is also described in the chemSHERPA manual.

"In case of error"

--> In case of error, please request again.