What is the difference between QR/P1-PCA2B-221 and QR/P1-PC2B-221(12) ?

Modified on Fri, Jun 19 at 12:57 PM

​The difference is the sequence contact.
QR/P1-PCA2B-221      : Sequence contact
QR/P1-PC2B-221(12)  : Not sequence contact

Applicator is the same.  Applicator part number is AP105-QR/P1-2B-2.
QR/P1-PCA2B-221 is sequence contact that contacts with the other connector first at mating,
when QR/P1-PCA2B-221 and QR/P-PC2B-221(12) are used together.
Both contacts can be used for QR/P1-**PC-C(50).
Note: ** stands for number of contacts. 
Example: QR/P1-16PC-C(50)(Scheduled to be discontinued).