What is the difference between HD-LN(05)(scheduled to be discontinued), HD-LN(08) and HD-LN(54) ?

Modified on Fri, Jun 19 at 1:00 PM

The difference is screw and spring washer.

HD-LN(05) : Applicable panel thickness = less than1.2mm(scheduled to be discontinued)
HD-LN(08) : Applicable panel thick ness =1.2mm - 1.6mm
HD-LN(54) : Without screw and spring washer.

Exterior plating for these 3 items is nickel.​