Are there any problems if the EF2 series connection moves because the cable moves left and right after insertion?

Modified on Fri, Jun 19 at 1:01 PM

No, it can be used without any problems.
In case of screw type terminal block, it is a problem because the screw loosens when cable moves, but there is no problem in case of the zero screw terminal block because of spring type. The reliability test was done to confirm.