What is the conditions to use UL20276 cable with DF52 series?

Modified on Fri, Jun 19 at 1:04 PM

​UL20276 core conductor specifications are the same of  UL1571 in case of AWG#28(gauge size).    So, the crimping condition is also the same.
https://www.hirose.com/product/document?clcode=CL0901-4636-7-00&productname=AP105-DF52-2832P&series=&documenttype=CrimpCondition&lang=ja&documentid=066802040_DF52A-2832PCFA(UL1571)_CC