Is S-16**A-J(50) the mating half cable extension case for P-16**A-CA(50)(Scheduled to be discontinued) ? ** stands for number of contacts.

Modified on Fri, Jun 19 at 12:49 PM

There is no extension cable jack case that mates with P-16**A-CA(50).  S-16**A-J(50)(Scheduled to be discontinued) is extension cable jack case but plug case that mates with is P-16**A-C(50). Please purchase connector units separately as these part numbers are cases only. The cases can be used for both male and female connector units.