What is the tolerance of applicable cable diameter of 9mm for JR13WCCA-9(72)?

Modified on Fri, Jun 19 at 12:53 PM

The outer diameter of the applicable cable of JR13WCCA-9(72) is 9 mm ± 0.5 mm as specified in the specifications. The difference between JR13WCCA-9(72) and JR13WCCA-9(31) that is listed on the catalog is material of waterproof packing.

JR13WCCA-9(31) : NBR (Nitrile rubber)
JR13WCCA-9(72) : SIR (Silicone rubber)