What is the insertion and withdrawal force when using PCN10EA-***S-2.54DSA(52) in combination with PCN10EA-***P-2.54DSA(72)(scheduled to be discontinued)?  *** stands for number of contacts.

Modified on Fri, Jun 19 at 12:55 PM

Insertion and withdrawal force are listed on the specification sheet of female connectors .

​Insertion force is 19.7N or less and
withdrawal force is 2.9N or more.