What is the difference between ER8-***P-0.8SV-2H and ER8-***P-0.8SV-2H(10)?  *** stands for number of contacts.

Modified on Fri, Jun 19 at 1:00 PM

The difference is contact plating.

ER8-***P-0.8SV-2H : 0.76μm gold over 2.54μm nickel, 
                              Thick plating is required for communication market. (Bellcore​ specification) 

ER8-***P-0.8SV-2H(10) : 0.25μm gold over 1.25μm nickel